AXIS#.IL.COMPTABLE.OUTPUT

Description

AXIS#.IL.COMPTABLE.OUTPUT returns the current output of the cogging compensation/torque compensation table.

See AXIS#.IL.COMPTABLE.DATA for more information how the table operates.

Versions

Action Version Notes
Implemented 02-07-03-000

General Information

Type

Read Only

Units

Arms

Range

AXIS#.IPEAK AXIS#.IPEAK

Index Range

N/A

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.COMPTABLE.OUTPUT

500ah

1eh

Signed16

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5843

1

5843 (0x16d3)

AXIS1.IL.COMPTABLE.OUTPUT

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.COMPTABLE.OUTPUT

5843

Float

Read Only

-